Read the KAS Manuals

If you prefer to read printed material, the following manuals (in PDF format) are available:

Document Title PDF Description
Release Notes The KAS version 3.07 Release Notes contain fixed limitations, known limitations, workarounds, and information on all hardware and software components that have been updated, changed or added in this release.
Getting Started

Covers the main steps to get your KAS system up and running.

30 Minutes to Motion Covers the main topics to help you start quickly with KAS IDEClosed "Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger. The objective is to familiarize you with the basic principles and the way the program works by creating a simple motion application project.
IDE User Manual Contains the content to help you with KAS IDE, except the topics included in the Reference Manuals.
Reference Manual - PLCClosed "Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events Library Contains Technical References on PLC Programming Languages and Library.
Reference Manual - Motion Library Contains Technical References on Motion Library for Pipe Network and PLCopenClosed A vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML.

Table 1-2: List of KAS Guides in PDF Format

See also the full list of deliverables here


  • The KAS IDE allows you to include references to external files such as the PDF files listed above. For more details, refer to Use the Reference Folder.

    Additionally, you can add in the PDF your own comments, tips and tricks, provided that you have Adobe Acrobat®.